2017-11-23 3:22 PM
Hi
I want to use dma and adc in such a way that the samples taken in a thousandth array are written. But this action only once and with my command, and then stop to issue the next command. Additionally, the adc speed is at its highest. Please guide me how to set the cubemx and what code to write. I apologize for the mistakes of sentences. I'm not fluent in English.
2017-11-27 8:31 AM
Please answer. tnks
2017-11-27 4:07 PM
do you have a sample cube file ?
its easy to do...
post your sample cube file here, I will show you the coding points / methodology
2017-11-27 6:41 PM
Hi
Thanks for answer
This is my cubemx and main.c file:
2017-11-27 8:17 PM
this is the code to get the data; I hacked this together, I have more than one channel running, my code is different
extern 'C' void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc){ HAL_ADC_Channel_Buffer [Counter] = ADC_DMABuffer[0]; Counter ++ &= 0xff;//256 byte buffer autoamtically loaded by the ADC callback } �?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
________________
Attachments : Sample F103C8 ADC.ioc.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyHR&d=%2Fa%2F0X0000000b5V%2FA.Og1waA6hJ0Fxhl0DmV7G_GIZG2sZ6gTDsY33mtATk&asPdf=false