ADC Analog Watchdog
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-02-22 4:39 AM
Posted on February 22, 2014 at 13:39
Hi All,
I have noticed that there are not much information in this forum regarding the subject.(stm32f4):0. Configure GPIO for ADC (PC0 - ADC channel 10) GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOC, &GPIO_InitStructure);1. Activate IRQ NVIC_InitTypeDef NVIC_InitStructure; NVIC_InitStructure.NVIC_IRQChannel = ADC_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); ADC_ITConfig(ADC1, ADC_IT_AWD, ENABLE);2. Configure ADC ADC_InitTypeDef ADC_init_structure; ADC_init_structure.ADC_DataAlign = ADC_DataAlign_Right; ADC_init_structure.ADC_Resolution = ADC_Resolution_12b; ADC_init_structure.ADC_ContinuousConvMode = ENABLE; ADC_init_structure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_init_structure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1; ADC_init_structure.ADC_NbrOfConversion = 1; ADC_init_structure.ADC_ScanConvMode = DISABLE; ADC_Init(ADC1, &ADC_init_structure); ADC_RegularChannelConfig(ADC1, ADC_Channel_10, 1, ADC_SampleTime_480Cycles);3. Configure AWD ADC_AnalogWatchdogSingleChannelConfig(ADC1, ADC_Channel_10); ADC_AnalogWatchdogThresholdsConfig(ADC1, 400, 0); ADC_AnalogWatchdogCmd(ADC1, ADC_AnalogWatchdog_SingleRegEnable);4. Activate ADC ADC_Cmd(ADC1, ENABLE);5. Set up IRQ function (everytime ) void ADC_IRQHandler(void) { if (ADC_GetITStatus(ADC1, ADC_IT_AWD)) { ADC_ClearITPendingBit(ADC1, ADC_IT_AWD); } }So every time the analog input pin gets a higher value than 400 the interrupt will fire.Is the configuration/statement correct above?Regards,/rygelxvi
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-02-23 7:09 AM
Posted on February 23, 2014 at 16:09
There are also a common config that perhaps needs to be addressed (that I missed before):
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent; ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_20Cycles; ADC_CommonInit(&ADC_CommonInitStructure); I found a good presentation for ADC that I have attached. Regards, /rygelxvi ________________ Attachments : Lecture_4-handout.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1MU&d=%2Fa%2F0X0000000bls%2FetFIUQ4Z5RtmUVXqbZX925pJ8Fx2gQItw4XyBSZO6hk&asPdf=false