cancel
Showing results for 
Search instead for 
Did you mean: 

About the STM32F769I-DISCO board, what are the maximum current consumption and the power input of the external connector ("JP1")?

LleytoN
Associate II

Hello!

I own an STM32F769I-DISCO board which presents an external connector called "JP1" (a picture of this one is given just below) used to power the microcontroller.

0693W00000HoQy0QAF.pngSo, I would like to know:

  • What is the maximum current consumption by this external connector?
  • What is the power input we could get here?

I truly thank you in advance for your help.

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

The current consumption depends very much on the respective application, but should generally be well below 500mA.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

The current consumption depends very much on the respective application, but should generally be well below 500mA.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
LleytoN
Associate II

Thank you very much for your answer!