About the output compare mode hunting
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-09-10 9:26 AM
Hello Person who knows the solution.
I am Yang and I try to make cluster for the rpm output but I met the rpm hunting problem. I need frequency modulation for the cluster. The below are the code than I use. STM32F407VG with 8HMz external clock and 168Mhz is system clock after PLL. I assign the PortC 4 for the output. When I check the output with oscilloscope, some times it shows very short pulse and it makes the rpm gauage jupm up. Is there something wrong in the STM32F407? I use ''STM32F4xx_StdPeriph_Driver''. I try to find the solution in the forum and I have a question about the ''stm32f4xx_tim.c''. void TIM_ClearITPendingBit(TIM_TypeDef* TIMx, uint16_t TIM_IT) { /* Check the parameters */ assert_param(IS_TIM_ALL_PERIPH(TIMx));/* Clear the IT pending Bit */
TIMx->SR = (uint16_t)~TIM_IT; } Is the command ''TIMx->SR = (uint16_t)~TIM_IT;'' correct? If I want to clear the TIM_IT position, ''TIMx->SR $= (uint16_t)~TIM_IT;'' looks correct.void timer5_set(void)
{ PrescalerValue = (uint16_t) ((168000000 / 2) / 500000) - 1;// Time base configuration //
TIM_TimeBaseStructure.TIM_Period = 65535; TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;TIM_TimeBaseInit(TIM5, &TIM_TimeBaseStructure);
// Prescaler configuration //
TIM_PrescalerConfig(TIM5, PrescalerValue, TIM_PSCReloadMode_Immediate);// Output Compare Timing Mode configuration: Channel1 //
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Timing; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = T3CCR1_Val; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;TIM_OC1Init(TIM5, &TIM_OCInitStructure);
TIM_OC1PreloadConfig(TIM5, TIM_OCPreload_Disable);// Output Compare Timing Mode configuration: Channel4 //
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = T3CCR2_Val;TIM_OC2Init(TIM5, &TIM_OCInitStructure);
TIM_OC2PreloadConfig(TIM5, TIM_OCPreload_Disable); // Output Compare Timing Mode configuration: Channel4 // TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = T3CCR2_Val;TIM_OC3Init(TIM5, &TIM_OCInitStructure);
TIM_OC3PreloadConfig(TIM5, TIM_OCPreload_Disable);// Output Compare Timing Mode configuration: Channel4 //
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = T3CCR2_Val;TIM_OC4Init(TIM5, &TIM_OCInitStructure);
TIM_OC4PreloadConfig(TIM5, TIM_OCPreload_Disable);//TIM Interrupts enable //
TIM_ITConfig(TIM5, TIM_IT_CC1 | TIM_IT_CC2 | TIM_IT_CC3 | TIM_IT_CC4, ENABLE);// TIM5 enable counter //
TIM_Cmd(TIM5, ENABLE); }void TIM5_IRQHandler(void)
{ if(TIM_GetITStatus(TIM5, TIM_IT_CC1) != RESET) { TIM_ClearITPendingBit(TIM5, TIM_IT_CC1); if(B_ig_on) GPIO_ToggleBits(GPIOD, GPIO_Pin_3); else GPIO_SetBits(GPIOD, GPIO_Pin_3);capture1 = TIM_GetCapture1(TIM5);
TIM_SetCompare1(TIM5, (u16)(capture1+cc1_val)); } else if(TIM_GetITStatus(TIM5, TIM_IT_CC2) != RESET) { TIM_ClearITPendingBit(TIM5, TIM_IT_CC2); if(B_ig_on) GPIO_ToggleBits(GPIOE, GPIO_Pin_1); else GPIO_SetBits(GPIOE, GPIO_Pin_1);capture2 = TIM_GetCapture2(TIM5);
TIM_SetCompare2(TIM5, (u16)(capture2 + cc2_val)); } else if(TIM_GetITStatus(TIM5, TIM_IT_CC3) != RESET) { TIM_ClearITPendingBit(TIM5, TIM_IT_CC3); if(B_ig_on) GPIO_ToggleBits(GPIOE, GPIO_Pin_3); else GPIO_SetBits(GPIOE, GPIO_Pin_3); capture3 = TIM_GetCapture3(TIM5); TIM_SetCompare3(TIM5, (u16)(capture3 + cc3_val)); } else if(TIM_GetITStatus(TIM5, TIM_IT_CC4) != RESET) { TIM_ClearITPendingBit(TIM5, TIM_IT_CC4); if(B_rpm) GPIO_ToggleBits(GPIOC, GPIO_Pin_4); // && B_ig_on else GPIO_SetBits(GPIOC, GPIO_Pin_4); capture4 = TIM_GetCapture4(TIM5); TIM_SetCompare4(TIM5, (u16)(capture4 + cc4_val)); } } Thank you. #stm32f- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-09-10 10:37 AM
The behaviour of TIMx->SR is documented in the Reference Manual
If you use TIMx->SR &= ~TIM_IT; you would cause a race hazard, remember AND'ing something you want to preserve with ZERO is always a bad plan. Consider if the amount you are advancing by is too tight. You don't mention a frequency and the code is insufficiently complete to infer one.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-09-11 1:17 AM
Thank you for your concerns.
I tried to start with original commands. TIMx->SR = ~TIM_IT; The frequency range is from 50Hz(1200rpm)~300Hz(7200rpm). cc4_val varis from 723 to 10551. Thank you