cancel
Showing results for 
Search instead for 
Did you mean: 

A warning about parity mode on the UART

DiBosco
Senior II
Posted on July 15, 2010 at 17:22

A warning about parity mode on the UART

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
t1
Associate II
Posted on May 17, 2011 at 13:58

Table 179 in revision 10 of the reference manual seems to be quite clear.

Did you see this table?

DiBosco
Senior II
Posted on May 17, 2011 at 13:58

Nope, mine is revision nine and table 179 doesn't mention it.

t1
Associate II
Posted on May 17, 2011 at 13:58

In revision 9, it is table 177.

In revision 1, it is table 68.

DiBosco
Senior II
Posted on May 17, 2011 at 13:59

This should be referenced from the register descriptions and I still think it's poorly worded (like much of ST's documentation, sadly).

swhite2
Associate III
Posted on May 17, 2011 at 13:59

This is something that could be handled by ST's Standard Peripheral Library USART module but isn't (in v3.3.0).

kashif
Associate II
Posted on May 17, 2011 at 13:59

thanks robert. i just read it before using nine bit protocol :)

and also agreed about the bad documentation of ST :( except firmware library user manual which is quite better