cancel
Showing results for 
Search instead for 
Did you mean: 

a specific pulse generation using the STM32 timers

hesam moshiri
Associate III
Posted on July 15, 2018 at 22:51

Hi,

I want to generate a pulse something like this and use it as a trigger internally, I mean I don't want to have this pulse on MCU pins and therefore I should use Timers. I want to use it as an ADC trigger. What should I do?

0690X0000060MCLQA2.jpg
2 REPLIES 2
henry.dick
Senior II
Posted on July 16, 2018 at 01:05

this identical question has pop'd up recently, more than a few times. the last one as i recall was by a self-proclaimed 'decent' programmer who failed at his attempt.

so a search can help you here.

Posted on July 16, 2018 at 06:25

I searched for that, unfortunately I could not find something special