2018-02-08 9:53 PM
ST is to be complimented for three specific design improvements apparent in the 769disco. FIrst, it actually has a connector to the display, rather than the LCD cable being soldered directly to the board, as is typical of the 429-disco and the 746-disco. This ought to make it much easier to upgrade the system. Furthermore, ST is actually making two versions of the 769-disco - one with a display, and one without, so we don't have to buy a system with a display, and then throw the display away because we are upgrading the system to a larger brighter display to be sunlight visible. The third is that the 769disco has mounting holes, as does the 746disco, where the 429disco has none. I have wanted all of those improvements with other systems we have bought from ST through distribution. Thanks for the progress ST!
However, I also have a question or two. One, I would like to see downloadable full system source kits including the CubeMx project file, for all boards, starting with the 769disco, of course! It would make it a lot easier to adapt the system, rather than having to puzzle out what device support is required. If you have not had to do that, lucky you. ST, please make this happen soon. You should find that to be dead easy, and VERY popular.
Two, I would like to see better stability in the product mix available. We shipped multiple 746disco units that we upgraded to 7' sunlight visible LCDs, and now find that there are no more 746disco units available here, and only electronic rumors of 87 being available at Newark UK. Newark in Canada has not be able to nail down their UK options for us to date. Digikey, Arrow, and Future have no stock of the 746disco at all. However, there are nearly 1000 pieces of the 769disco available, so we are checking out the 769disco because we are forced to, not because we want to.
I am sure we can be criticized for having shipped systems with xxx-disco units, and be told that we should have built our own boards to ship. However, if what ST is doing with chips is good, what is wrong with using their boards too,
instead of only using their board designs? If what you are doing is selling, figure out how to sell more of it, and keeping stock in the distribution channels sounds like a good move. Dropping product availability significantly makes the marketplace wonder what is really happening.
If you agree or disagree with the points above, say so. If enough of us encourage ST in the right direction, they might actually go there!
Dan
#downloadable-full-source-kits #stability-of-product-mix2018-02-10 4:56 PM
only 1 in stock, its the H753 the big brother to everyone... with Crypto
Enlarge
https://au.mouser.com/images/icon-lc-new-product-sm.png
New Producthttps://au.mouser.com/stmicroelectronics
Development Boards & Kits - ARM Evaluation board with STM32H753XI MCUhttps://au.mouser.com/stm-stm32h753xi-board
https://www.mouser.com/ds/2/389/en.DM00378466-1149pdf
1
In Stock$689
Min.: 1
Mult.: 1
2018-02-10 5:48 PM
1215 of what in stock? 746G-disco? They have 0 in stock, and 1215 on order, with first projected delivery March 28.
That's not very interesting, until we get to March 28.
2018-02-10 5:51 PM
If I am going to contract for a batch, then I want changes, because the existing design is needs changes. If I am buying a few, then I can accept what is. And if I am going to wait for changes, then I want the design files as well. We are using Pulsonix. What are you using?
2018-02-10 6:28 PM
oh, im not using anything. ive never done this before in my life. im just totally willing to seize the opportunity on the off chance you're willing to do the right thing.
2018-02-10 6:56 PM
How much is the Pulsonix PCB software, they don't show it on the site.
2018-02-10 7:27 PM
Off Chance? Thanks a lot! If you've never done it before, the risks should be carefully considered - especially in making changes....
2018-02-10 7:28 PM
Say about $3000 Canadian. Not interested in eval machines - too expensive.
2018-02-11 2:05 AM
Sorry it was late. You're right. Even RS says probably 03/13.
2018-02-11 2:15 AM
I would sell my 746-DISCO (B2B) and can ship immediately .
Honestly, I don't need it because I put the focus on the 769-DISCO.
Probably you'll find other guys as well.
2018-02-11 7:23 AM
Well the original F7 offering was always pretty sad given the competition released a better CM7 (FPU-D, 300 MHz) from the outset.
I might suspect that ST has stepped the die used in the F746 to address some of the errata, and the dearth of boards relates to a flushing of old stock.
To be honest I prefer the F769I-DISC1 currently too, the Ethernet PoE being quite appealing. Although all the boards I have are A step parts.
Would check with FAE's, I'd imagine a couple of boxes of F746I-DISCOs floating around.