74HC595 8 Bit Shift Register with stm32f4discovery help
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-12-18 3:33 PM
Hi, I am a complete novice to the stm32f4discovery, I have made a 8x8 RGB led matrix using 4
74HC595 8 Bit Shift Registers with only 3 wires going to my now fried arduino, from the old arduino pins I had the 74HC595 8 Bit Shift Registers connected like this; DS to datapin, ST_CP to latchpin, SH_cp to clockpin, what pins do I use on the stm32f4discovery? Are they pd8 (TX), pd9 (RX), pd10 (CK)? if anyone know please could you tell me I wouldn’t like to fry another board :
Thanks for any help
Marin.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-12-18 4:20 PM
You'll also need to connect a GND wire for this to work.
Do you plan to drive the pins in GPIO mode? Would RX be appropriate? These 3 pins sound like outputs (Data, Clock, Latch).Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-12-18 4:39 PM
hi, I had 5v & GND coming from the arduino too, pins 8 10 11 were connted to the 74HC595 pin 8 was - clock, pins 10 and 11 were pwm from the arduino, just want to use the same outs from the stm32f4discovery but dont know which pins to use, I only ask because this stm32f4discovery is a replacement for my broken arduino and would like to use the rgb led matrix I had built for it.
the LEDs are multiplex'dcheers Martin.edit to add:this is the same design I used, the video is not mine and belongs to the owner of it, I'm just using it to show you how I had my old arduino running the LED'shttp://www.youtube.com/watch?v=j6nK33QI-So&context=C3adb5b2ADOEgsToPDskIQTPlKNFbxWwC4ySLV2DI-
I'm thinking about getting another arduino but thought I would give the stm32f4 a go, and try out 32bit- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-12-18 6:22 PM
I asked if you were planing on using the pins as GPIOs because the USART3 peripheral is probably not going to get the clocking/latching working in the manner you want.
If you don't want to ''bit-bang'' the GPIO's in question, which would work btw, then using one of the SPI peripherals might be a better choice to make the hardware do the donkey work. You could get the SPI to send four 8-bit bytes, or two 16-bit words, and after each group was sent (via DATA/MOSI + CLOCK) you could latch. This assumes you have the 4 8-bit shift registers daisy-chained end-on-end.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-12-19 8:17 AM
Hi sorry for the delay, yes my plan was to use the GPIO. as the 74HC595 will be doing all the work.
Martin.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-12-19 10:50 AM
Hi sorry for the delay, yes my plan was to use the GPIO. as the 74HC595 will be doing all the work.
Actually the STM32 CPU will be doing a lot of the grinding. So the you'll need to configure the pins as GPIO outputs, after enabling the clocks on the GPIO bank. You will then have to sequence/drive the pins in the prescribed order to get your serial stream of bits into the scan chain, and then latch them.Up vote any posts that you find helpful, it shows what's working..