cancel
Showing results for 
Search instead for 
Did you mean: 

How to use CD4094BE with 74HC595 shift registers

Bkris.2
Associate II

Hi Experts,

I have a project like below. I am trying to send the data but the LEDS are not glowing in sending pattern.

I am new to STM32F207 Nucleo board. Could anyone please let me know if I am missing anything.

STM32f207 ======> CD4094(Q0) ==========> 74HC595 =====> LEDS (1 to 8)

            (Q1) ==========> 74HC595 =====> LEDS (1 to 8)

(Q2) ==========> 74HC595 =====> LEDS (1 to 8)

                    

Code Snippet::

===============

uint8_t test[8]= {1,1,1,0,1,0,1,1};

uint8_t output=0,count =0;

for(int row=0;row<8;row++)

{

  HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET);/*STROBE PIN */

  count = 0;

  for(int bit=0;bit<8;bit++)

  {

   if(count>6)/* TO DISPLAY FIRST 8 LEDS IN 74HC595(Q0)*/

    {

   output = test[row] & 0X1;

    }

    else

    {

     output = 0;

    }

  count = count+1;

  if(output)

  {

   HAL_GPIO_WritePin(GPIOC, GPIO_PIN_4, GPIO_PIN_SET);/*DATA PIN */

  }

  else

  {

   HAL_GPIO_WritePin(GPIOC, GPIO_PIN_4, GPIO_PIN_RESET);

  }

  HAL_GPIO_WritePin(GPIOC, GPIO_PIN_5, GPIO_PIN_RESET);/*CLK PIN */

  HAL_Delay(1);

  HAL_GPIO_WritePin(GPIOC, GPIO_PIN_5, GPIO_PIN_SET);

  HAL_Delay(1);

  }

   HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_SET);

   HAL_Delay(1);

}

WORKING SCNERAIO 

=================

STM32f207 ======> CD4094(Q0-Q7) =====> LEDS (1 to 8)

uint8_t test[8]= {1,1,1,0,1,0,1,1};

uint8_t output=0,count =0;

  HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET);/*STROBE PIN */

  count = 0;

  for(int bit=0;bit<8;bit++)

  {

  if(count>5)/* TO DISPLAY FIRST 2 LEDS IN 4094*/

    {

   output = test[row] & 0X1;

    }

    else

    {

     output = 0;

    }

  if(output)

  {

   HAL_GPIO_WritePin(GPIOC, GPIO_PIN_4, GPIO_PIN_SET);/*DATA PIN */

  }

  else

  {

   HAL_GPIO_WritePin(GPIOC, GPIO_PIN_4, GPIO_PIN_RESET);

  }

  HAL_GPIO_WritePin(GPIOC, GPIO_PIN_5, GPIO_PIN_RESET);/*CLK PIN */

  HAL_Delay(1);

  HAL_GPIO_WritePin(GPIOC, GPIO_PIN_5, GPIO_PIN_SET);

  HAL_Delay(1);

  }

   HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_SET);

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0