429I-DISCO PWM output
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-12-03 8:01 PM
Hi,
I'd like to output 30kHz PWM from PA5, but following code won't work. What is wrong with this code?#include ''stm32f4xx.h''
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;uint16_t CCR1_Val = 350;
uint16_t PrescalerValue = 0;void TIM_Config(void);
int main(void)
{ GPIO_InitTypeDef GPIO_InitStructure;RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);/* GPIOA Configuration: TIM2 CH1 (PA5) */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ; GPIO_Init(GPIOA, &GPIO_InitStructure);GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_TIM2);
RCC_TIMCLKPresConfig(RCC_TIMPrescActivated);
PrescalerValue = (uint16_t) (SystemCoreClock / 21000000) - 1;
TIM_TimeBaseStructure.TIM_Period = 699;
TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = CCR1_Val; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;TIM_OC1Init(TIM2, &TIM_OCInitStructure);
TIM_OC1PreloadConfig(TIM2, TIM_OCPreload_Enable); TIM_ARRPreloadConfig(TIM2, ENABLE); TIM_Cmd(TIM2, ENABLE);while (1) {}
} This code was modified from Peripheral_Examples on stsw-stm32138, If the setting is original TIM4 CH1 PD12, then it was working well. tyro- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-12-04 12:26 AM
My god, I found that I always checked
PA7
instead ofPA5.
I must return to my office for signal checkbecause
there is oscilloscope. 429I-DISCO does not print the pin name at one side of P1 and P2, so I had thought that PA5 must be next to PA4, but it has reverse sequence against an actual pin numbers.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-12-04 1:40 AM
Solved. PWM output from PA5 was working well.
tyro