2020-08-02 8:06 PM
Dear Members,
How can I get exactly 1Hz interrupt from TIM3 ?
I use STM32F4 Discovery and looking at TIM_TimeBase Example, but I can not get exactly 1Hz yet...
Thanks
Code :
TIM_OCInitTypeDef TIM_OCInitStructure;
__IO uint16_t CCR1_Val = 54618;
__IO uint16_t CCR2_Val = 27309;
__IO uint16_t CCR3_Val = 13654;
__IO uint16_t CCR4_Val = 6826;
/* -----------------------------------------------------------------------
TIM3 Configuration: Output Compare Timing Mode:
In this example TIM3 input clock (TIM3CLK) is set to 2 * APB1 clock (PCLK1),
since APB1 prescaler is different from 1.
TIM3CLK = 2 * PCLK1
PCLK1 = HCLK / 4
=> TIM3CLK = HCLK / 2 = SystemCoreClock /2
To get TIM3 counter clock at 50 MHz, the prescaler is computed as follows:
Prescaler = (TIM3CLK / TIM3 counter clock) - 1
Prescaler = ((SystemCoreClock /2) /50 MHz) - 1
CC1 update rate = TIM3 counter clock / CCR1_Val = 9.154 Hz
==> Toggling frequency = 4.57 Hz
C2 update rate = TIM3 counter clock / CCR2_Val = 18.31 Hz
==> Toggling frequency = 9.15 Hz
CC3 update rate = TIM3 counter clock / CCR3_Val = 36.62 Hz
==> Toggling frequency = 18.31 Hz
CC4 update rate = TIM3 counter clock / CCR4_Val = 73.25 Hz
==> Toggling frequency = 36.62 Hz
/* Compute the prescaler value */
//PrescalerValue = (uint16_t) ((SystemCoreClock / 2) / 500000) - 1;
PrescalerValue = (uint16_t) ((SystemCoreClock / 2) / 6826) - 1; //TIM3 counter clock at 6826Hz
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Period = 65535;
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
/* Prescaler configuration */
TIM_PrescalerConfig(TIM3, PrescalerValue, TIM_PSCReloadMode_Immediate);
/* Output Compare Timing Mode configuration: Channel1 */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Timing;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = CCR1_Val;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OC1Init(TIM3, &TIM_OCInitStructure);
TIM_OC1PreloadConfig(TIM3, TIM_OCPreload_Disable);
/* Output Compare Timing Mode configuration: Channel2 */
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = CCR2_Val;
TIM_OC2Init(TIM3, &TIM_OCInitStructure);
TIM_OC2PreloadConfig(TIM3, TIM_OCPreload_Disable);
/* Output Compare Timing Mode configuration: Channel3 */
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = CCR3_Val;
TIM_OC3Init(TIM3, &TIM_OCInitStructure);
TIM_OC3PreloadConfig(TIM3, TIM_OCPreload_Disable);
/* Output Compare Timing Mode configuration: Channel4 */
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = CCR4_Val;
TIM_OC4Init(TIM3, &TIM_OCInitStructure);
TIM_OC4PreloadConfig(TIM3, TIM_OCPreload_Disable);
/* TIM Interrupts enable */
TIM_ITConfig(TIM3, TIM_IT_CC1 | TIM_IT_CC2 | TIM_IT_CC3 | TIM_IT_CC4, ENABLE);This example shows how to configure the TIM peripheral in Output Compare Timing
mode with the corresponding Interrupt requests for each channel in order to generate
4 different time bases.
The TIM3CLK frequency is set to SystemCoreClock / 2 (Hz), to get TIM3 counter
clock at 500 KHz so the Prescaler is computed as following:
- Prescaler = (TIM3CLK / TIM3 counter clock) - 1
SystemCoreClock is set to 168 MHz for STM32F4xx Devices Revision A.
The TIM3 CC1 register value is equal to 54618,
CC1 update rate = TIM3 counter clock / CCR1_Val = 9.154 Hz,
so the TIM3 Channel 1 generates an interrupt each 109.2ms
The TIM3 CC2 register is equal to 27309,
CC2 update rate = TIM3 counter clock / CCR2_Val = 18.31 Hz
so the TIM3 Channel 2 generates an interrupt each 54.6ms
The TIM3 CC3 register is equal to 13654,
CC3 update rate = TIM3 counter clock / CCR3_Val = 36.62 Hz
so the TIM3 Channel 3 generates an interrupt each 27.3ms
The TIM3 CC4 register is equal to 6826,
CC4 update rate = TIM3 counter clock / CCR4_Val = 73.25 Hz
so the TIM3 Channel 4 generates an interrupt each 13.65ms.
When the counter value reaches the Output compare registers values, the Output
Compare interrupts are generated and, in the handler routine, 4 pins(PD.12, PD.13,
PD.14 and PD.15) are toggled with the following frequencies:
- PD.12: 4.57 Hz (CC1)
- PD.13: 9.15 Hz (CC2)
- PD.14: 18.31 Hz (CC3)
- PD.15: 36.62 Hz (CC4)
2020-08-04 9:03 PM
Like this :
__IO uint16_t CCR1_Val = 3000;
__IO uint16_t CCR2_Val = 6000;
__IO uint16_t CCR3_Val = 12000;
__IO uint16_t CCR4_Val = 60000;
.
.
.
PrescalerValue = (uint16_t) ((SystemCoreClock / 2) / 3000) - 1; //TIM3 counter clock at 3000Hz
.
.
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Period = 65535;
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
.
.
.
void TIM3_IRQHandler(void)
{
if (TIM_GetITStatus(TIM3, TIM_IT_CC1) != RESET)
{
TIM_ClearITPendingBit(TIM3, TIM_IT_CC1);
/* LED4 toggling with frequency = 4.57 Hz */
STM_EVAL_LEDToggle(LED4);
capture = TIM_GetCapture1(TIM3);
TIM_SetCompare1(TIM3, capture + CCR1_Val);
}
else if (TIM_GetITStatus(TIM3, TIM_IT_CC2) != RESET)
{
TIM_ClearITPendingBit(TIM3, TIM_IT_CC2);
/* LED3 toggling with frequency = 9.15 Hz */
STM_EVAL_LEDToggle(LED3);
capture = TIM_GetCapture2(TIM3);
TIM_SetCompare2(TIM3, capture + CCR2_Val);
}
else if (TIM_GetITStatus(TIM3, TIM_IT_CC3) != RESET)
{
TIM_ClearITPendingBit(TIM3, TIM_IT_CC3);
/* LED5 toggling with frequency = 18.31 Hz */
STM_EVAL_LEDToggle(LED5);
capture = TIM_GetCapture3(TIM3);
TIM_SetCompare3(TIM3, capture + CCR3_Val);
}
else
{
TIM_ClearITPendingBit(TIM3, TIM_IT_CC4);
/* LED6 toggling with frequency = 36.62 Hz */
STM_EVAL_LEDToggle(LED6);
capture = TIM_GetCapture4(TIM3);
TIM_SetCompare4(TIM3, capture + CCR4_Val);
}
}
2020-08-05 12:06 AM
You still have set prescaler to 65'536. That's why you are getting 65'536 / 28'000 = 2,34 Hz instead of 1 Hz and some other x2 factor which turns it into 4,68 Hz.
CCR3_Val is not set to 0,1 Hz. Compare value = timer_clock (Hz) / compare_frequency (Hz).
2020-08-05 3:33 PM
do you mean :
TIM_TimeBaseStructure.TIM_Period = 65535;
?
Timer clock = 3000 Hz and compare frequency = 0.5 Hz
CCR3_Val is a variable on TIM3_IRQHandler
Compare Value = 3000 Hz / 0.5 Hz
2020-08-06 6:43 AM
__IO uint16_t CCR1_Val = 3000/1;
__IO uint16_t CCR2_Val = 3000/0.25;
__IO uint16_t CCR3_Val = 3000/0.125;
__IO uint16_t CCR4_Val = 3000/0.062;
?
2020-08-20 10:56 PM
Is it possible that I have 1s interrupt then for getting 60 seconds, I loop that 1s , 60 times ?
Where can I put that loop ?
if (TIM_GetITStatus(TIM3, TIM_IT_CC1) != RESET)
{
TIM_ClearITPendingBit(TIM3, TIM_IT_CC1);
/* LED4 toggling with frequency = 4.57 Hz */
STM_EVAL_LEDToggle(LED4);
capture = TIM_GetCapture1(TIM3);
TIM_SetCompare1(TIM3, capture + CCR1_Val);
}
Call the loop function here ?Thanks