cancel
Showing results for 
Search instead for 
Did you mean: 

X-Nucleo-IHM03A1

Janusz53
Associate

Good morning

I am in the process of building another CNC milling machine. For the two largest stepper motors , I would like to use X-Nucleo-IHM03A1 drivers connected to the Stm32 board. I initially looked at the capabilities of IHM03A1 and batch files for Stm32CubeIDE.

I have a question:

Can IHM03A1 be controlled via Stm32 board from an external motion controller , for example by providing an external PULSE signal to the STCK pin ?

Thank you in advance

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Janusz53, to the community!

Which STM32 board did you connect the X-NUCLEO-IHM03A1  to? If it is a NUCLEO board, you should be able to use it to control the X-NUCLEO?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.