2021-07-10 5:47 AM
I want to drive a BLDC Motor using STM32F103C8T6. The said controller is not present in the official support of X-Cube-MCSDK. I want to understand how we can add a new STM32 MCU in the X-Cube-MCSDK. Also, I want to understand does the X-Cube-MCSDK supports 6xPWM. The reason I am asking about 6xpwm compatibility because what I could understand from the X-Cube-MCSDK is that it outputs 3 pins as PWM and 3 pins as enable/disable[GPIO not as PWM]
2021-07-19 1:23 AM
Dear @Community member
I am not sure I understood your question.
If you want to know if our solution can control a 6 phase motor instead of three, the answer is no.
If you want to know if our solution can drive high sides and low sides transistors, the answer is yes.
Otherwise, please rephrase your question.
Best regards
2021-07-19 4:02 AM
Dear @Community member
Is it answer to your question?
Best regards