cancel
Showing results for 
Search instead for 
Did you mean: 

Why the start of ovm mode is set to these value?

Konecho
Associate II
#define OVM_VREF_MODE1_START ((int32_t)29717)
#define OVM_VREF_MODE2_START ((int32_t)31186)

The ratio between these two value is not sqrt(3)/2. What is the voltage unit used in these calculation? Or when a have a Valpha equal to 32767, what is the truth voltage in real world?

 

Thanks.

2 REPLIES 2
Konecho
Associate II

Also, the document "A priori determination of flux and torque current PI gains" says that the PI module uses a voltage factor of VBusDC/2^16, is this correct?Seems like it should be 3VBusDC/2^16.

Konecho
Associate II

Found something interesting:

the PI controller and FF think the voltage reference is Vbus/2,

the PWMC_SetPhaseVoltagefunction thinks it's Vbus/sqrt(3),

PWMC_SetPhaseVoltage_OVM thinks it's 2Vbus/3,

circle limit in OVM mode thinks it's -- 2Vbus/pi, right?