cancel
Showing results for 
Search instead for 
Did you mean: 

Using timer 3 to read hall sensors

SLori.1
Associate II

I’m trying to use the timer3 ch1 ch2 ch3 of stm32g4 to read the hall sensors of motor but selecting this config under workbench 5.y. the motor doesn’t work. The default hall sensors timer is timer2. Any idea?

This discussion is locked. Please start a new topic to ask your question.
23 REPLIES 23
Hi Cedric, what is the max power motor (current) that the X-NUCLEO-IHM16M1 can manage? Like nominal and in rush Current ecc? For which kind of motor is thought? Many thank Br Il giorno lunedì 4 ottobre 2021, ST Community ha scritto:
SLori.1
Associate II

Hi Cedric, what is the max power motor (current) that the X-NUCLEO-IHM16M1 can manage? Like nominal and in rush Current ecc? For which kind of motor is thought? Many thank

Br

SLori.1
Associate II

Hi Cedric, what is the max power motor (current) that the X-NUCLEO-IHM16M1 can manage? Like nominal and in rush Current ecc? For which kind of motor is thought? Many thank

Br

cedric H
ST Employee

Hello @SLori.1​ ,

unfortunately, I can not provide you more information than one present in the specification available here for the board :

https://www.st.com/resource/en/data_brief/x-nucleo-ihm16m1.pdf

And here for the STSPIN830 :

https://www.st.com/resource/en/datasheet/stspin830.pdf

So :

IOUT,RMS Continuous power stage output current (each bridge) 1.5 Arms

Regards

Cedric