2020-07-15 06:04 PM
2021-06-28 05:36 AM
Dear @PBoni.1304 and @Vdsfg.1
There is now in the last SDK version a demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.
Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .
Best regards
2020-07-20 02:19 AM
dear Vdsfg.1,
I am sorry, we have not such library so far... It's part of our roadmap but not before 2021.
Thanks,
Claire
2021-03-24 01:34 PM
News about ACIM Motors support for "FOC SDK"?
2021-06-15 12:38 AM
The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK).
Best regards
2021-06-28 05:36 AM
Dear @PBoni.1304 and @Vdsfg.1
There is now in the last SDK version a demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.
Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .
Best regards