cancel
Showing results for 
Search instead for 
Did you mean: 

SVPWM and BEMF Wareform type

Vincent7
Associate

Hello Everybody,

MCSDK:6.3.0

CubeMX: 6.3.0

Workbench : 6.3.0

Motor Pilot : 1.2.9

Power Board : IHM08M1

Control Board : NUCLEO-G431RB

Motor : GBM2804H-100T

I am currently testing FOC-OpenLoop-Voltage. I am using Motor Pilot for tuning and measuring SVPWM (at OUT1~OUT3) and BEMF (at D6, D8, D10) with an oscilloscope. However, both waveforms appear as square waves. Could this be related to the specific motor model I am using?

0 REPLIES 0