2015-12-02 05:05 AM
Hello,
i want to generate a project with the WB for an existing hardware. But i can't configure the Ports for the 2 Analog Inputs of the Shunts. Can you help me to configure the project? Hardware: STM32F405 Gate Driver DRV8302 with Amplifiers for two Shunts (1mOhm)2016-01-07 08:58 AM
Ciao Eric
You can select in the ST MC Workbench the two insulated current sensing as Current Sensing Network into the Power Stage section, then you have to select the two ADC input in the Control Stage -> Analog Input section. Ciao Gigi2021-06-17 01:12 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards