2018-09-11 8:13 PM
I use Lib version 4.3 to control SM-PMSM.
The motor can run smoothly.
However I would like to simulate 2 error hereafter.
I would like to check these 2 error without modify code.
PS.I have locked rotor when start ,it shows under-power error instead of Start up fail.
2021-06-28 3:06 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards