2021-11-17 07:48 PM
Hello,
I'm just getting started with STM32 and got my hand on STEVAL-SPIN3202. I did follow the manual and install X-CUBE-MCSDK, stsw-link009 driver and everything the manual suggested. However, I couldn't get the workbench to regcognize the board and keep getting the error "Connection fail! no response, check the communication cable, the power on the board or the baudrate".
I did look around in this forum and realized this is a common occurance. However, even though I making sure setting the workbench baudrate, Digital I/O parameter and Device manager comport baudrate to 9600, the problem still persist. I did re-generate the code everytime I change the parameters so I don't know the cause of the problem anymore.
Best Regard.
2021-12-20 10:57 PM
Dear @KCham.2
Sorry for the late answer.
Do you have still this problem to solve?
And just in case, if not, do not hesitate to share the final solution you found. Thanks by advance.
Best regards
2021-12-21 12:44 AM
Dear @Laurent Ca...
Thank you for responding. I still couldn't get the board to work so I decided to hold it off for the time being. If you have any idea on the solution, I'd really appreciate it.
Sincerely