2019-04-16 08:45 AM
STEVAL-SPIN3201
I have a motor connected to this board and just cannot get it to run correctly.
I get the start up error or speed feedback error when running the motor.
I am running the motor in sensor less mode using the sample software (SDK5x - STEVAL-SPIN3201 - BullRunning.stmcx) with adjusted parameters.
I get the motor to startup (appears to be correct) but then when it reaches target rpm it the fails (most of the time with startup error)
I am using ST motor control Workbench, STM 32 Cube and IAR
Please can you assist with getting the motor to actually spin.
2021-06-14 11:52 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards