2021-04-21 8:22 AM
This is the first time in this forum and want to start working on the ST micro controller. My main aim is
a. Buy high end ST evaluation kit and understand the FOC algorithm for PMSM motors. The kit should contain the motor along with evaluation kit.
b. I get the source code with the kit and modify the source according to my requirements.
Request to please suggest me a motor control evaluation kit.
Thanks in advance
Solved! Go to Solution.
2021-04-26 6:01 AM
yes, checkout this https://www.st.com/en/embedded-software/x-cube-mcsdk-ful.html
2021-04-21 8:27 AM
P-NUCLEO-IHM001 is convenient and it worked fine for me.
(if youre fine with that tiny motor)
https://www.cnx-software.com/2015/09/29/stmicro-introduces-35-stm32-motor-control-nucleo-pack/
2021-04-22 7:52 AM
Thank you for the reply. Yes it is a tiny motor, are there other boards with high power rating you can recommend?
Few other questions
Please help.
2021-04-26 2:55 AM
@VD.3
I tried STEVAL-IPM15B and i gave up trying to make it work.
So i dont recommend thatone.
2021-04-26 5:55 AM
Thank you for the reply, hopefully final question i searched for the software source code, does ST provide the source code for FOC and the driver software's to run these evaluation boards or we need to develop from the scratch?
2021-04-26 6:01 AM
yes, checkout this https://www.st.com/en/embedded-software/x-cube-mcsdk-ful.html