2019-11-06 10:20 PM
I have made a SM-PMSM project for a hub motor (10 pole pairs). I can compile the generated code in STM32CubeIDE (HAL) but when I run it I always get the fault "Speed feedback" in Motor Control Workbench Monitor.
There is 20ms of activity, where there is 3ms of 13kHz PWM wave from about zero to nominal voltage (p-p) at 50% duty, then "Speed feedback" fault occurs. The waveforms are identical on all phases. The motor does not move, therefore no encoder pulses.
It is strange that the pulse are the same on all three phase outputs, basically stalling the motor.
What is going on here?
UPDATE:
Is there a way to test the STEVAL-SPIN3201 board?
UPDATE 2:
The motor control SDK user manual (UM2392) mentions this fault "The speed feedback is not reliable any more (usually happens when the rotor speed goes too low)"
But at this stage I am not even trying to have a low speed.
Hmmm!?! Anyone got any ideas?
Solved! Go to Solution.
2023-07-21 10:21 AM
How exactly were you able to get it run in Sensorless? You mentioned you increassed the current on the start-up, but how much, in terms of motor spec current, did you increassed? Can you share the configurations made at your side?
I'm trying hard to make it run on a 17" SM-PMSM on a custom driver board. On startup, the motor tryies to spin but it shorts and the MCU reset. On that point the MCU reset and reads no signal from the hall sensors, so it stops and flags "Speed feedback" fault.
Already calculated the electrical angle for the 120° hall sensors mounted on the motor.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.