Problem to compile my project with Motor Control Workbench
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-05-19 2:48 AM
Good morning, I can’t compile my project to use the Motor Control Workbench 4.3 Monitor
I summarize the initial process: Open Workbench, New Project, select Power and control after select NUCLEO-F303RE and STEVAL-IPM05F 3Sh and a my custom motor profile.
Now can Save my project, use this folder:
C:\Program Files (x86)\STMicroelectronics\FOC SDK\v4.3.0\STM32 PMSM FOC LIB\Web
After set all motor, power stage, Drive management and Control Stage parameters, save the project.
Press “generation�? and select the default folder. Now it’s appear a pop-up to remember to program my nucleo. I will use AC6, I open this file:
C:\Program Files (x86)\STMicroelectronics\FOC SDK\v4.3.0\STM32 PMSM FOC LIB\Web\Project\AC6\STM32F30x_UserProject/.project
AC6 start, I will compile but I can select 4 option but none for my STM32F303.
When I try to compile there are a 2 problem:
#error 'Invalid configuration: MCU definition in Control stage parameters.h not compatible with selected board. Please use the ST Motor Control Workbench to configure the firmware according your system.' STM32F30x_UserProject line 88, external location: C:\Data\Software\STM32\Workbench\Web\Project\CrossCheck.h
make: *** [UI Library/src/UserInterfaceClass.o] Error 1 STM32F30x_UserProject
what am I doing wrong?
Thanks
Manuele
- Labels:
-
STM32 Motor Control
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-10-17 5:49 AM
I am having the same problem only with IAR as IDE. There is no option to select F303RE in the drop-down menu for compilation and download/debug.
There is only:
STM32F30x_UserProject - STM32303C-EVAL_SINGLEDRIVE
STM32F30x_UserProject - STM32303C-EVAL_DUALDRIVE
STM32F302_SINGLEDRRIVE
P-NUCLEO.IHM001_SINGLEDRIVE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-06-15 1:53 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards