2017-05-23 10:57 PM
Hello, All:
I use (ST Motor control Workbench) parameters in power management where I set up some flow parameters, and then generate the file in Power stage, But I did not find the parameters.h file to set my parameters, why, where is it?
/*********** Over-current protection section ************/
#define OVERCURR_FEEDBACK_POLARITY EMSTOP2_ACTIVE_LOW #define OVERCURR_PROTECTION_HW_DISABLING DOUT_ACTIVE_HIGH/************************************************* ************/
There is no parameter about overcurrent.
Thank you!
2021-06-27 06:39 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards