2023-04-18 2:56 PM
I plan to start using the MC SDK, and I was ready to get a Nucleo-G474RE with a IHM16M1.
But when looking at the motor profiler utility, I noticed that the combination is not supported. There is support for the IHM16M1 and the STM32G474 processor in the STM32G474E-EVAL, but not for the combination I'd like to use.
II also checked in the firmware directory, but there is no hex file for my desired combination.
Is there a way to build the firmware for the profiler? If not, any plan to support the combination? I really would like to avoid buying a different Nucleo board, as I wanted to use the opportunity to learn more about the STM32G4 family
2023-04-26 8:56 AM
Anyone? Is there a better forum to ask this question?
2024-05-09 2:17 AM
Did you get any further on your own since you didnt get any answer?
I too want to get the motor profiler running with the exact same setup as you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.