cancel
Showing results for 
Search instead for 
Did you mean: 

Motor drive product recommendation

TRowe
Associate II

Hi, I have an electric assist power steering column I have been working on building a control module for. It uses a 630w IPMSM motor with hall sensors and has a supply voltage of 12-14V DC. I have managed to get the motor to run with a G431-ESC1 and use an arduino to monitor steering sensor outputs and send a pwm to the esc. It does work but the motor is not producing enough torque for adequate steering assist. I assume this is because the G431-ESC1 is really not powerful enough to run a motor of this size. Can anyone recommend a product in the stm32 range that might be suitable. At this point I’m looking at the STEVAL-CTM009V1 but wondering if there’s something closer to what I require.

Thanks, Tony

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
GMA
ST Employee

Hello,

Please try motor control solution  link which gives an overview.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA