cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Control PMSM FOC user projects location

imtiaz
Associate II
Posted on April 11, 2016 at 23:47

Hi ,

I am unable to locate the user projects after installing the Motor Control SDK. Can any one tell me where I can find the user projects that interact with the FOC library - specifically I need the Keil uVision ones.

In the installation folder :

C:\Program Files (x86)\STMicroelectronics\FOC SDK\STMCWBv4.2\ExampleProjects\WB_Projects\SDK42x -ther are onl;y .stmcx projects - no keil uvision or EWarm projects

Thanks for your help

#stm32-pmsm-mc-library-user-proje
3 REPLIES 3
imtiaz
Associate II
Posted on April 12, 2016 at 00:15

To answer my own question for someone elses benefit - the prjects are in :

C:\Program Files (x86)\STMicroelectronics\FOC SDK\STM32 PMSM FOC LIBv4.2\Web\

Gigi
ST Employee
Posted on April 12, 2016 at 10:37

Ciao

I'm happy that you find the solution.

To be precise the project are in the folders

C:\Program Files (x86)\STMicroelectronics\FOC SDK\STM32 PMSM FOC LIBv4.2\Web\Project\EWARM for IAR

and

C:\Program Files (x86)\STMicroelectronics\FOC SDK\STM32 PMSM FOC LIBv4.2\Web\Project\MDK-ARM for Keil

Ciao

Gigi

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards