cancel
Showing results for 
Search instead for 
Did you mean: 

motor control in STM32 cortex M0

motor_control
Associate
Posted on September 14, 2014 at 21:48

Hi,

would like to use STM 32 F0 for 3-phase motor control. Could anyone please let me know what evaluation board for motor control in STM32 F0 to purchase?

ALso, I

noticed that st’s library

"

STM32 PMSM FOC SDK

"

supports STM32 F0 as well

.

How does it work?

Thanks and best regards

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Gigi
ST Employee
Posted on September 22, 2014 at 11:13

Ciao Motor

The evaluation board that you can find in the ST stock that is based on STM32F0 is the

http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/LN1199/PF259717?s_searchtype=partnumber

but up to now the STM32 PMSM FOC SDK motor control firmware library

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1734/PF257936?s_searchtype=partnumber

 support ''out-of-the-box'' the STM320518-EVAL, the older one that is now no more at stock.

We plan to extend the support of the STM32072B-EVAL in the next release of the SDK.

Ciao

Gigi

cnmountain
Associate II
Posted on September 24, 2014 at 01:29

Thanks a lot, Gigi.

I checked

http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/LN1199/PF259717?s_searchtype=partnumber

, but it doesn't look to support motor control friendly. Since there is no main circuits (rectifier) included on this EVM. what else I need to be cautious when choosing a main circuit?

Also, Is this easier to use discovery kit directly connected to main circuit? 

 

http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF253215?sc=internet/evalboard/product/253215.jsp

It is great to hear that ST is going to support STM32072B-EVAL with FOC. When do we expect to be available?

Gigi
ST Employee
Posted on September 24, 2014 at 08:47

Ciao Motor

I don't know if I catch your question. To build a motor control system you have two choice:

- Arrange a system with a Control Board plus a Power Board

- Try with a single board approach

With the first you have the flexibility to choose the computational power of the micro + the power size of the inverter.

The STM32072B-EVAL is just a control board and you have to combine it with any power board (STEVAL-IHM0xx) present in the ST stock.

Discovery kit is not supported by the FOC SDK and can't be connected with the power board because there is no 34pin MC connector onboard.

The next release of the FOC SDK will support the STM32072B-EVAL and is planned for Q1 '15

Ciao

Gigi

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards