2017-12-14 6:03 PM
Hi
Now I tried to activate Low Voltage BLDC Motor(Model : Shinano LA052-080E3NL1) using by 'STM32F PMSM single/dual FOC SDK v4.3'.
The hardware configuration is following below :
Control Board : STM32303C-EVAL
Power Stage : STEVAL-IHM023V2
BLDC Motor : LA052-080E3NL1
As follow instruction in user manual, I could activated BLDC Motor.
in this point, I have some questions about FOC SDK 4.3.
question 1)
But, BLDC Motor couldn't run in low speed using by sensorless FOC Control and sixstep control method.
Is it avoidable problem of BLDC Motor or did I something miss?
question 2)
What is the ''Stop Ramp'' function in monitor of ST Motor Workbench?
I didn't see this function working when I click that button. even it dosen't exactly descrived in user manual.
question 3)
is there exist 'sensored FOC control of BLDC' in 'STM32F PMSM single/dual FOC SDK v4.3'?
Thanks.
#foc-sdk-4.3.0 #bldc2021-06-21 10:43 PM
The question has been moved to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards