2021-08-23 2:08 AM
Dear Team,
In a project for our client we are selected an ST solution for time saving and for reliability as per the previous interaction between us. But now we are in a great trouble and asking for your support on same.
I am in need of your support now the issue is
Other setting provided with Motor Profiler
1. DC Connected 12 V adapter 1 A
2. Pole pair 7
3. Max Speed 12000 rpm
4. Max Current o.96 APK
Its working and profiler shows following results
a. Imax 0.9 Apk
b. Rs 0.51 ohm
c. Ls 0.03mH
d. VBus 11.6V
e. Ke 0.76 Vrms/kRPM
f. Friction 189.76 nN m s
g. Inertia nN-m-s2
h. Max Speed 11970 Rpm
? My first question is that I can found some warning symbol on electrical model. Is there anything wrong with my settings
? I tried with Motor Control workbench with some default examples for FOC speed control but the result was not promising. No movement is happening to motor can u help me in same?
? can u send me a ready to use code for this, I am asking this because I had already spend two weeks of time on this?
2023-08-29 12:45 AM - edited 2023-08-29 12:45 AM
Hello @KR.4 ,
We would like to sincerely apologize for the delay in replying to your post.
If your point is still pertinent, can you try with MCSDK 6.1.2 and let me know if that solves your problem?
Regards