cancel
Showing results for 
Search instead for 
Did you mean: 

ioc file not generated from Motor Control Workbench - template inclusion failed

KStew.1
Associate II

Using Version: 6.3.2

I have a custom motor and a custom inverter board, importing these works fine in my project but when I try to generate the project I get the following:

2025-03-17 17:54:58,571 ERROR [LineInfo_to_exitCode.manage_IocGenerationError] Unable to generate ioc file due to: Template inclusion failed (for parameter value "STM32F769NI/STM32F769NI - 216 MHz - int.ftl"):...

I tried changing the MCU on my inverter to see if this was specific to a board and I keep getting the same bug. Please help :)

 

0 REPLIES 0