2023-09-26 08:05 PM
I often use Motor Profiler to identify motors.But it is not good.
Sometimes my motor cannot be recognized when using 48V and I have to reduce the supply voltage to 36V.
Here I would like to ask whether it will be open sourced. I want to understand the principle of identifying the motor and improve it.
Solved! Go to Solution.
2023-09-27 12:53 AM
Hello @gtop.1
To answer your main question, there are currently no plans to make the Profiler opensource. to let me better understand your problem to help you find a solution: Can you tell me which version of the MCSDK you are using? and which power board and control board do you use ?
Thank you
2023-09-27 12:53 AM
Hello @gtop.1
To answer your main question, there are currently no plans to make the Profiler opensource. to let me better understand your problem to help you find a solution: Can you tell me which version of the MCSDK you are using? and which power board and control board do you use ?
Thank you
2023-09-27 09:06 PM
Hello.
I use 5.Y.4 MCSDK and NUCLEO-F302R8+X-NUCLEO-IHM08M1 3Sh,with 48V 471W pmsm motor. The motor keeps turning and cannot identify the Ke.
2023-09-28 05:08 AM
Can you try with the new version of MCSDK 6.2, and tell me if it works better. To use the profiler on 6.2 you must generate a profiler firmware, for this please follow the MCSDK documentation.
2023-10-08 01:38 AM
Yes,it works better. It can work in 48V now.
I want to kown how to calculate the Ke.
I refer here:https://wiki.stmicroelectronics.cn/stm32mcu/wiki/STM32MotorControl:How_To_manually_configure_the_motor_parameters
Below is the profiler's result. Ke=9.59 Vrms/kRPM.
Below is my owm test.
Vpp=13.6v,pole pairs=5,fbemf=83.33Hz. Ke=(13.6*5*1000)/(2√2*83.33*60)=4.8085 Vrms/kRPM.
I wonder if I chose the wrong frequency?Is it between point A and point B or pointA and pointC?Thanks.
2023-10-08 02:00 AM
Add a picture
2023-10-09 01:36 AM
hi @gtop.1
Can you mark your first question as answered, and make a new post for your new question please? this will allow us to have better follow-up of questions
regards
2023-10-09 03:13 AM
ok