cancel
Showing results for 
Search instead for 
Did you mean: 

I am able to generate a complementary PWM signal. However due to hardware changes I would need to add a dead time. Regardless the value I am setting in the BDTR register there is no dead time at the output.

Handzic.Dirk
Associate III

// Initialisation

TIM1->PSC = (FOSC/(PWM_FREQ * PWM_STEPS)) - 1;    // Timer clock

TIM1->ARR = PWM_STEPS - 1;                        // Auto reload

TIM1->BDTR = 0;                                    // Safety

TIM1->CCER = 0;

TIM1->CR2 = 0;

TIM1->CCMR1 = TIM_CCMR1_OC1M_1 | TIM_CCMR1_OC1M_2 | TIM_CCMR1_OC2M_1 | TIM_CCMR1_OC2M_2;   // PWM mode 1 on channel 1 and 2

 // PWM mode 1 on ch 3 for ADC sample trigger 

TIM1->CCMR2 = TIM_CCMR2_OC3M_1 | TIM_CCMR2_OC3M_2;         

TIM1->CCR3 = SAMPLE_POINT;            

 // Turn all outputs off

 TIM1->CCER = 0;

//Starting PWM

TIM1->EGR |= TIM_EGR_UG;               

TIM1->CCMR1 = TIM_CCMR1_OC1M_1 | TIM_CCMR1_OC1M_2 |TIM_CCMR1_OC2M_0 | TIM_CCMR1_OC2M_2;        // Channel 1 pwm Force channel 2 high

TIM1->CCER |= TIM_CCER_CC1E | TIM_CCER_CC1NE | TIM_CCER_CC2E | TIM_CCER_CC2NE | TIM_CCER_CC3E; //

TIM1->CR2 = TIM_CR2_OIS1N;

TIM1->BDTR = TIM_BDTR_MOE |(DTGMULT_8 | DTG_VAL); 

 TIM1->CR1 = TIM_CR1_CEN;                           // Start timer

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Handzic.Dirk
Associate III

Found the problem! The above code works but I thought the tDTG would be FOSC/PSC but it seems to be based on a higher frequency. How can tDTG be calculated?