2018-04-18 04:51 PM
Hello,
I recently bought two BLDC motor controllers, the STEVAL-SPIN3202 and the X-NUCLEO-IHM08M1 shield forNUCLEO-F401RE.
I have a project to control a BLDC sensored motor. I am not sure how to move forward. I have AC6, IAR and MKD installed. I have tried installed motor control workbench with no luck. X-CUBE-MCSDK executable that can be downloaded from the following link does not work for some reason.
http://www.st.com/en/embedded-software/stsw-stm32100.html
I am wondering if there is something else I need to install for this to work?
FIY, I am using Windows10 and I have STM32CubeMX installed.
Solved! Go to Solution.
2021-06-27 06:28 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards