2018-04-18 4:51 PM
Hello,
I recently bought two BLDC motor controllers, the STEVAL-SPIN3202 and the X-NUCLEO-IHM08M1 shield forNUCLEO-F401RE.
I have a project to control a BLDC sensored motor. I am not sure how to move forward. I have AC6, IAR and MKD installed. I have tried installed motor control workbench with no luck. X-CUBE-MCSDK executable that can be downloaded from the following link does not work for some reason.
http://www.st.com/en/embedded-software/stsw-stm32100.html
I am wondering if there is something else I need to install for this to work?
FIY, I am using Windows10 and I have STM32CubeMX installed.
Solved! Go to Solution.
2018-04-19 12:46 AM
It seems that the X-CUBE-MCSDK package is actually a zip file and not an exe.
If Windows complains that 'The version of this file is not compatible with the version of windows you're running' Try to unzip the file first. It should be fixed in the coming hours...
2018-04-19 12:46 AM
It seems that the X-CUBE-MCSDK package is actually a zip file and not an exe.
If Windows complains that 'The version of this file is not compatible with the version of windows you're running' Try to unzip the file first. It should be fixed in the coming hours...
2018-04-19 3:19 PM
Thank you for your help.
You are correct. I changed the file domain to zip, and when I unzipped it, another executable showed up. I was able to run that, and it seems the problem is fixed on the server side as well.2018-04-20 9:06 AM
hi Abdul,
Have you succeed in installing and generating the code for motor control ?
2018-04-20 10:29 PM
Yes, I managed to install it, but I haven't tried it out yet.
2018-04-21 1:35 AM
Thanks
Could you me please let me know if code generation is successfully working ? I am fed of trying to generate code, but I having some problems in generating the code. (with mcsdk 5.0.2 or 5.0.3)
thanks a lot Abdul...
2018-04-21 5:03 PM
Hello gokay,
I think I managed to generate the STM32CubeMX project. I can't test this with my motor as the motor control program does not include the STM32F401RE board, which what ST recommends for the NUCLEO-IHM08M1 shield. The project does open using STM32CubeMX. I already tried to compile ''as-is'' with IAR and failed. I am going to try make it work without the motor control workbench software.
What boards do you have btw?
For what is supposed to be a plug-and-play setup, this is kind of frustrating.
2018-04-21 5:08 PM
I am not sure if this will work, but maybe try with the older version 4.3?
2018-04-23 3:26 AM
Dear Abdul,
I understand your frustration. The message around the support of the IHM08 is not very clear.
There is actually two kinds of software solution in order to control a BLDC motor :
- 6 steps
- FOC
The 6 steps software solution for IHM08 can be downloaded here :
It supports the IHM08+STM32F401RE or IHM08+STM32F302R8.
The FOC software solution (
X-CUBE-MCSDK ) does not support the
STM32F401RE in the 5.0.3 version. It was not supported in the 4.3 version too.
We plan to add the support of the STM32F401RE in X-CUBE-MCSDK 5.1 version.
Could you tell me in case of FOC, what is your configuration ? 1 Shunt - 3 shunts ?
Regards
Cedric
2018-04-23 1:50 PM
Hi Cedric
Let me say this. I really appreciate your help on this matter. Just to give you little bit of background. I have a 250W BLDC motor for a mobile robot. my aim is to run it around 0-300 rpm, so relatively low speed. It's a sensored motor with 3 hall effect, 2 optical, and temperature sensors. The supply voltage is between 42 and 30 volts (10S Lipo).
Based my research, I understand that sensored FOC would be a better fit for me, but I don't care about efficiency at the moment. I don't care if it's sensored or sensoreless drive. I just want to operate the motors using the
SPIN3202 or
IHM08M1 with the easiest setup possible. From a specification standpoint, they both seem to able meet my needs.
The boards that I have currently are the STM32F401RE and STM32F446RE. I bought the F401 specially for the
IHM08M1
shield, but it's not listed in the ST motor control workbench software.I am looking into the code you provided in the link. There is a similar one for the SPIN3202. What I am trying to do right now, is to understand the code so I can start manually editing it. I knew I had to do this eventually, but I just thought there might be an ''out of the box'' solution, that is temporary until I make improvements myself. I sort of got motor spin one rotation, but I think it's designed for motors with RPM > 2000, so I need to fix that.
Again thank you for you help.
On a side note, I don't have the datasheet for the motor, so I was going to use the motor profile. I found out the F4xx series isn't supported, so I might buy a F3xx board. I am wondering if you have a recommendation? I can see the F303RE and F302R8 listed in the software.