2020-05-27 09:40 AM
This is a basic question but has me stumped. I have an existing motor project with a *.stmcx file. I generated a new *.xml file for the motor using the profiler. How do I get the *.xml file converted over to a new *.stmcx file? I can load the existing project in the Motor Control Workbench but it doesn't give an option to load a new motor file .....
2021-06-21 10:28 PM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards