How to configure pinout and clock in a project without .ioc file ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-03-15 9:31 AM
Hello,
I am working with a NUCLEO-F446RE development board and an X-NUCLEO-IHM06A1 motor control board to control a stepper motor.
An example project (STM32CubeExpansion_SPN6) is given with the motor board. However, I want to modify this project to add two PWM outputs and UART communication.
Normally I would do this by modifying the .ioc file, but it is not provided in the example project. Is there any way to recreate the .ioc file? If not, how can I do the PIN configuration? What are the names of the files in which this configuration is found?
Thanks in advance,
Best regards,
Yoan
- Labels:
-
STM32 Motor Control
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-03-16 8:35 PM
Hello @YNL_95,
What you can do is generate the code you need for your PWM and UART using STM32CubeMX and then copy it to your example project.
Regards,
Ryan