cancel
Showing results for 
Search instead for 
Did you mean: 

Help with Reducing Power Usage in STM32F423ZHT6 Smart Lock

mabubilal
Associate

Hey all,
I'm using the STM32F423ZHT6 for a Smart Lock with 2 limit switches for lock/unlock. The problem is, the motor stays on all the time, so it’s using a lot of power. Any tips on (https://faisalmoversonline.pk/) how to reduce this? I want the motor to run only when needed.

1 ACCEPTED SOLUTION

Accepted Solutions
3 REPLIES 3
Andrew Neil
Evangelist III

Do you think you've presented details of the 'design' that are adequate to understand what you've built?

If this is a class project, please work with your teacher or supervisor.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

@Tesla DeLorean wrote:

If this is a class project, please work with your teacher or supervisor.


^^^ Always this! ^^^

@mabubilal is @Meenakshi your classmate, on the same project? If so, you should collaborate ...