2024-09-28 04:37 AM
Hey all,
I'm using the STM32F423ZHT6 for a Smart Lock with 2 limit switches for lock/unlock. The problem is, the motor stays on all the time, so it’s using a lot of power. Any tips on how to reduce this? I want the motor to run only when needed.
2024-09-28 04:53 AM - edited 2024-09-28 04:53 AM
2024-09-28 06:12 AM
Do you think you've presented details of the 'design' that are adequate to understand what you've built?
If this is a class project, please work with your teacher or supervisor.