2025-03-18 1:42 AM
Hello,
I need confirmation that the Hall Delay in the below waveform i have taken is 180Degrees. Hall sensors are 120Degrees apart as below in the diagram
I find the motor running in reverse direction.
2025-03-24 6:40 AM
Reverse direction could mean that you have a misalignment between motor phases and hall sensors. Try reversing 2 phases and the motor will spin in the correct direction
2025-03-26 9:45 AM
Hello @STUser34,
Using Motor Workbench 6.3.2, you can take the advantage of Hall Sensor Motor Profiler.
Refer to User Manual documentation available through "Workbench tool">About>Documentations>Documentation>"User manual" tab>"Motor Profiler Application Note" link for more detail.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.