cancel
Showing results for 
Search instead for 
Did you mean: 

Generating project files using ST Motor Control Workbench resulted in an error

Lzj111111
Associate II

I'm currently encountering an issue with the P-NUCLEO-IHM001 motor. I'm using STM32Cube version 6.10 and X-CUBE-MCSDK version 5.4.8. During file generation, the problem shown in the image has arisen. How should I resolve this?

*This post has been translated from Chinese to comply with the ST Community guidelines.

1 ACCEPTED SOLUTION

Accepted Solutions
GMA
ST Employee

Hello @Lzj111111,

The language of the Community is English as mentioned here.

Refer to the MCSDK5.4.8 release note for the STM32 environment. You must first install STM32CubeMX v6.4.0 and the expected STM32Cube_FW_F3_V1.11.3 firmware package (in your image, it is mentioned as expected but not installed).

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

View solution in original post

3 REPLIES 3
GMA
ST Employee

Hello @Lzj111111,

The language of the Community is English as mentioned here.

Refer to the MCSDK5.4.8 release note for the STM32 environment. You must first install STM32CubeMX v6.4.0 and the expected STM32Cube_FW_F3_V1.11.3 firmware package (in your image, it is mentioned as expected but not installed).

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

After following your instructions, I encountered the error shown in the image. How should I resolve this? Thank you.

*This post has been translated from Chinese to comply with the ST Community guidelines.

GMA
ST Employee

Hello @Lzj111111,

If the project generation finishes with the generation of the main.c file, proceed with the generated project.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA