STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1716 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9546 Views
  • 5 replies
  • 3 kudos

Stepper Control with l6474

Hi, @Peter BENSCH . I am working on a project. In which i need to control Stepper motor using X-Nucleo-IHM01A1 Sheild. Currently i'm using STM32G431RB Nucleo-64 board for this and in future will use STM32F103. I've download X Cube SPN1 for basic work...

SannanAli by Associate II
  • 1842 Views
  • 6 replies
  • 1 kudos

Resolved! No ACIM example in MCSDK 5.4.7 or 5.4.8

Hello ST community.Based on the content of this page, there should be ACIM example files for V/F and FOC motor drives, but after downloading both MCSDK 5.4.7 and 5.4.8, i found no ACIM example file for this topic in MC Workbecnch. Where shoud i get t...

Amirmhz by Associate II
  • 331 Views
  • 1 replies
  • 0 kudos

Resolved! Config Motor parameter without recompile

Hello. I am trying to develop a BLDC motor driver. With Workbench, I can easily change the motor parameter. But whenever I change the motor, I should reconfigure and re-compile. So I would like to make a FW can change motor parameter dynamically. Is ...

DonCC007 by Associate
  • 885 Views
  • 2 replies
  • 0 kudos