Skip to main content
SF??r
Associate III
September 10, 2024
Question

Formular of Feed Forward Control Constants

  • September 10, 2024
  • 1 reply
  • 656 views

Hi,

 

the MotorControlWorkbench is generating the Feedforward control constants:

M1_CONSTANT1_Q

M1_CONSTANT1_D

M1_CONSTANT2_QD

How are the calculated, are there any documentation or formula for it?

The Feedforward seems to be relevant for my project because I see current ripple aligned with my DC bus voltage ripple. But in practice there is no improvement, if I activate the FeedForward control. Also the bus voltage is measured with 1 ms and a filter with 6 values is applied. Are there any tips for my application if I have a bus voltage ripple period of 10 ms (3 Phase, 50 Hz)?

 

Thanks for Help

 

Sebastian 

    1 reply

    roar
    Associate II
    January 13, 2026

    Also interested in how these constants are calculated. Did you find any information on this?

     

    Regards

    Roar