2019-10-27 10:09 AM
Hi i have configured the quadrature encoder in Motor->Sensors and set the number of pulses
and select the quadrature encoder in Drive Management->Speed/Position Feedback Management
for to finish set the correct IO pins used for the quadrature encoder in Control Stage->Digital IO. as A15 and B3.
After this, compile and load, but the motor does nos espin , what i have done wrong ?
Thanks
2021-06-14 11:41 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards