2016-10-03 8:37 AM
I see in RN0085 that the FOC libary v4.3 is listed. In new features for v4.3 I see AC6 workspace. Yay! this is great for us. We want to use the STM32 Open Development Env. as a base for all our firmware.
Please can you give details on when will v4.3 be released? Chris #foc-4.3 #stm32-ode2016-10-11 12:08 AM
Ciao the new version is not released yet, we are still in qualification phase.
In few week probably we will have it published.
Ciao
Gigi
2021-06-28 2:32 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
2021-06-28 2:43 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards