cancel
Showing results for 
Search instead for 
Did you mean: 

FOC 4.3 filename issue

John HU
Associate
Posted on February 26, 2018 at 04:00

FOC 4.3 lib use filename with space, like

Control stage parameters

Parameters conversion

Parameters conversion F0xx

PMSM motor parameters

Power stage parameters

But it is not user friendly for some windows tools.

Would you please change _ style , like

Control_stage_parameters

Parameters_conversion

Parameters_conversion_F0xx

PMSM_motor_parameters

Power_stage_parameters

...

thanks a lot

1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards