2024-07-11 04:04 PM
Hi,
I am confused on how I can get this board: EVLDRIVE101-HPD, to work.
For context, I am simply trying to get the EVLDRIVE101-HPD to run a compressor motor.
From my understanding, I believe I need to generate the code/firmware through MCSDK workbench and then compile the code through an IDE (im using STM32CubeIDE) into the EVLDRIVE101-HPD board with the STM32G071KBT. However, both softwares do not have the board (EVLDRIVE101-HPD) as an option in the setup.
I have the board's JSON file which I believe can be imported in the MCSDK workbench but need further instructions on how?
Could I please have some general help with this? As well as clear instructions on how to get this board to work with my motor?
Any help will be appreciated. thanks!