2016-04-20 10:52 AM
Hello, I am trying to evaluate motor control firmware with AC6 Workbench. I am looking at the STM32 PMSM FOC SDK 4.2, Hands-on workshop with hardware tools, Rev 1.5, and it only supports Keil and IAR. Is there a version for AC6 Workbench?
Thanks.2016-04-20 11:31 PM
Ciao
No I'm sorry. At the moment the workspaces for AC6 is not provided with the last release of the MC FOC Lib. Ciao Gigi2021-06-17 12:37 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards