2019-07-02 7:37 PM
Hello Community,
I have purchased a STEVAL-SPIN3201 eval board last week. I want to drive a 48V Drum motor using this eval board with Motor Control Workbench 5.40. But I don't have the full motor parameters. Based on the user manual UM2152, the motor parameter configuration need to modify if different motor application is used and then generate new firmware code download into the eval board. My question is anyone tried this kind of motor using Motor Control Workbench 5.40. If yes, can you share how's the configuration
The motor information below is all I have:
Rated voltage: 48V
Rated current: 6A
number of Poles: 10
Thanks.
Regards,
XH Low
2019-07-09 9:39 AM
2019-07-10 12:42 AM
Thanks Cedric.
Let's see I can measure the motor parameters.
Regards,
XH Low
2021-06-22 1:26 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards